The current carrying capacity of cables is one of the decisive selection parameters, especially in the field of energy transmission, or for classic motor and servo cables. The DIN VDE 0298-4 says amongst other things:“The current carrying capacity is the maximum permissible current under certain conditions at which the conductor is not heated above the permissible […]
In the early days of Covid-19, our daily companion today, there was great uncertainty. In the health care system in particular, people were afraid that there were not enough ventilators. At that time, we at igus were thinking intensively about how we could provide support here, in a cost-sensitive manner. Especially as our lubrication-free high-performance […]
In order to be able to exploit all the advantages, a certain degree of order is also required for small connector components. This requires a way to easily fasten or securely install round connectors. And this is exactly what such plug holders are for.
At customers’ premises, I often observe how the electricians unwind cables from the cable reels or remove them from the cable ring in various ways during installation. You can go wrong here. Especially when the cable concerned is used for dynamic applications in energy chains, incorrect unreeling can have fatal consequences. To be honest, when […]
Guide cables and hoses safely in limited installation space without rapid fatigue fractures that lead to expensive downtime: an ultimate discipline! The possibilities offered by compact energy chains and highly flexible cables. Building a house in the country, on a 1,000m2 plot: no problem. It gets trickier in a 200m2 small gap in a big […]