April, 2020 - igus Blog - Page 16 April, 2020 - igus Blog - Page 16

Crane main power and data supply, proven and alternative systems

Theo Diehl | 9. April 2020

For crane main power and data supply a motor cable drum or – for short travels – a spring tension drum is usually used. Busbar systems for the main power supply are also very common in indoor cranes. As an alternative to the two solutions, an energy chain can be used, which can offer various advantages.

Read more...

Cost-effective plain bearings in electric coolant pumps and regulators

Sebastian Bloechl | 9. April 2020

The demand for electric water pumps is huge. In addition to the cooling of motors and drives, air conditioning is also one of its tasks. The advantages of electric coolant pumps compared to conventional mechanical water pumps are their independence from the combustion engine. In this way, the electric pumps can be switched on and […]

Read more...

Machines and plant for plastics processing. An industry overview.

Christian Schäfer | 9. April 2020

The plastics processing industry is manifold. Whether in injection moulding machines, blow moulding machines, extruders or presses, plastics are processed into very different products. The igus products can be found in a variety of machines and equipment for the plastic and rubber industry.

Read more...

Cable guide for load suspension device on an indoor crane

Jens Göbel | 9. April 2020

liftband was specifically developed for vertical applications on indoor cranes. A spiral-shaped energy chain that can be placed in a collection basket. The cables are guided in the spiral-shaped energy chain without any tensile strain. The straps attached to the system ensure that the energy chain remains safe in the collection basket. The system is light, requires very little installation space on the load suspension device and is virtually maintenance-free.

Read more...

Why plastic sliding rollers? Part 2

Bastian Mehr | 9. April 2020

What can be done with a plastic sliding roller? Here we must clearly compare the cost-benefit factor. Basically, a solid plastic roller is a cost-effective component: of course, depending on the material and the production process behind it. But the plastic roller has its limits. Here one must assess whether the application is suitable. With […]

Read more...