Video - igus Blog - Page 15 Video - igus Blog - Page 15

Keyword:

Video

robolink passes function test in rough vacuum (TU Munich)

Martin Raak | 20. October 2011

Technical University of Munich, Department of Aerospace Engineering – LRT – tests the joint in rough vacuum and certifies full functionality. Experimental conditions according to the attached certificate, test set-up documented in the film. Anwender_Info_TUM_LRT_komplett_EN.pdf   Vote Up +0 Vote Down -0You already voted!

Read more...

robolink double articulated arm – speed test

Martin Raak | 23. September 2011

The high speeds of the robolink joint are tested with this testing system. The four degrees of freedom of the double joint are accelerated to an angular velocity of 150°/s. The average speed of the mounted weight (560 g) is thereby 1.05 m/s. Vote Up +0 Vote Down -0You already voted!

Read more...

New trade fair site – Application in coolants/lubricants

Martin Raak | 19. September 2011

The application of robolink in machine tools and the influence of coolants/lubricants is demonstrated here. Vote Up +0 Vote Down -0You already voted!

Read more...

Asymmetric robolink-version

Martin Raak | 28. July 2011

Asymmetric pivot angle arrangement: Displacement of the pivot angle of +/-90° to +130°/-50° This gives you a completely new area of operations with our robolink multi-axis joints. All other properties do not change compared to the original version. Both versions can be freely combined as desired. Get an overview in the following video. Vote Up […]

Read more...

Angular sensor

Martin Raak | 1. June 2010

angular sensor Due to the integrated angular sensors, an arm can also be used directly as “teach-in” arm. Read-out angle information can be saved and called up or even directly transformed into movements (see film). Currently the sensor technology is advanced for series production. Development partner EvoLogics GmbH is a specialist for bionic inventions (the […]

Read more...