Polymer ball bearings - igus Blog - Page 3 Polymer ball bearings - igus Blog - Page 3

Keyword:

Polymer ball bearings

Ball bearings in ATMs: polymer excels here as well

Patrick Czaja | 25. November 2020

ATMs are among the igus® xiros® ball bearings applications. Our polymer ball bearings fully demonstrate their superiority to metallic ball bearings in these applications. xiros® radial deep groove ball bearings are advantageous because they not only require no maintenance or lubrication, but also eliminate lubrication contamination on banknotes.

Read more...

Which ball bearing seals are available and why doesn’t igus need additional markings

Patrick Czaja | 13. November 2020

Many metallic rolling bearings are available as a sealed version Ball bearing seals are usually mandatory for the metallic version, otherwise dirt will get into the running surfaces of the ball. They can combine with the lubricant and block the bearing run. Ball bearings made of polymer or ceramic are mostly only available as an open type. Why? Find out here.

Read more...

How do I find out the DIN installation size of the metal ball bearing? And how do I find the igus® counterpart?

Patrick Czaja | 11. November 2020

For metallic ball bearings, determining the installation size is usually simple. Usually the type designation is printed either on the inner or outer ring. It becomes more difficult, however, if the imprint remains unrecognisable despite cleaning. Therefore the ball bearing must be measured manually at this point. _x000D_   I now know my ball bearing […]

Read more...

The time for heating begins: polymer ball bearings from igus® defy extreme heat

Patrick Czaja | 27. October 2020

Plastics and hot temperatures in ovens do not have to oppose each other, as shown in the following application example of the Koppe company. Because lubrication-free polymer ball bearings from igus are successfully used in their pellet stoves for private households. The functionality of the stoves is ingenious, as the pellets burn without electricity via a mechanical drive unit. The polymer ball bearings ensure long running times and smooth operation in the drive unit.

Read more...

Slewing ring ball bearings from igus® for the most diverse applications

Patrick Czaja | 15. October 2020

ISAS GmbH also quickly realised that xiros is the best alternative for comparable metal solutions. This application case from the furniture industry shows you not only the requirements of ISAS GmbH, but also the numerous advantages of xiros slewing ring ball bearings made of polymer.

Read more...