Plastic ball bearings - igus Blog - Page 2 Plastic ball bearings - igus Blog - Page 2

Keyword:

Plastic ball bearings

igus® impresses with ball bearings in hose pumps

Patrick Czaja | 17. December 2020

The general requirements for the bearing components used in medical and food technology are extremely high and are subject to high quality standards. For example, in medical diagnostics such as dialysis, it is important to have components that are 100% free of lubricating greases or oils in order to keep the application sterile and clean.

Read more...

Ball bearings in the textile industry – why plastic beats metal

Patrick Czaja | 10. December 2020

Textile machines and their components are increasingly exposed to heavy loads. This increases the demands on the machines. Vibrations, different operating conditions, constantly changing loads and especially dirt and dust adhesion are challenges faced by plant operators in the textile industry.

Read more...

Ball bearings in anemometers – plastic makes measuring wind easy

Patrick Czaja | 8. December 2020

An anemometer is an instrument for measuring the speed of a flow field and is used primarily to determine wind speed. The cup anemometer is the most widely used type. It has a vertical axis with three or four cups to catch the wind. What requirements apply to ball bearings in anemometers?

Read more...

Ball bearings in copy machines: Why xiros® is the right choice

Patrick Czaja | 4. December 2020

Polymer ball bearings are being used more and more frequently in copy machines. Why? They are lubrication-free, low-maintenance and extremely lightweight. No external lubrication is necessary and contamination of the application environment can be ruled out.

Read more...

Ball bearings in ATMs: polymer excels here as well

Patrick Czaja | 25. November 2020

ATMs are among the igus® xiros® ball bearings applications. Our polymer ball bearings fully demonstrate their superiority to metallic ball bearings in these applications. xiros® radial deep groove ball bearings are advantageous because they not only require no maintenance or lubrication, but also eliminate lubrication contamination on banknotes.

Read more...