Plain bearings - igus Blog - Page 9 Plain bearings - igus Blog - Page 9

Keyword:

Plain bearings

Cost-effective plain bearings in electric coolant pumps and regulators

Sebastian Bloechl | 9. April 2020

The demand for electric water pumps is huge. In addition to the cooling of motors and drives, air conditioning is also one of its tasks. The advantages of electric coolant pumps compared to conventional mechanical water pumps are their independence from the combustion engine. In this way, the electric pumps can be switched on and […]

Read more...

New material iglidur® K250 in automotive applications

Julio Pauli | 9. April 2020

Wear results of our new material iglidur® K250, which is characterised by a high flexibility and moisture absorption, are presented below. Compared to the igus classic iglidur® M250, the tribological properties could also be improved.

Read more...

Coolant and plain bearings – five decisive points

Sebastian Bloechl | 7. April 2020

Maximum vehicle efficiency requires harmonised thermal management. Optimum operating temperature ensures efficiency and thus the lowest consumption and associated emissions. Coolant plays an important role – it cools, provides corrosion protection and prevents frost. Coolant pumps, regulators and valves distribute coolant throughout the vehicle, sending it where it is needed. Find out more here.  In […]

Read more...

Why is thermal management becoming more and more significant for the automobile industry?

Sebastian Bloechl | 2. April 2020

Cosy heating in the winter and an air-conditioned living room in the summer – in addition to such everyday concerns, thermal management plays a decisive role in the automotive industry. In that industry, for instance, it is the engine that meets various scenarios. At first, it needs a temperature rise that is as quick as […]

Read more...

The right shaft for tough outdoor use – if the plain bearing is outdoors.

Uwe Sund | 31. March 2020

Everyone knows that the agricultural and construction machinery sector require lots of care. Dirt, moisture, corrosion, the complete package. Whether a combine harvester, tractor, concrete mixer, plough or mobile crane – here everything is in the same boat. Metallic plain bearings are always lubricated – at least they should be if they are to function. […]

Read more...