Plain bearings - igus Blog - Page 3 Plain bearings - igus Blog - Page 3

Keyword:

Plain bearings

Plain bearings for high speeds? Where are the limits?

Lars Butenschön | 10. December 2021

“Plain bearings are particularly suitable for high loads at low speeds.” This, or something similar, is what many technical books, guides, and also advertising texts say. There are two things about this statement that are not particularly helpful in practice. This blog post will analyse this statement and the conditions under which certain types of […]

Read more...

Correctly select piston rings

Lars Butenschön | 12. November 2021

As with most machine components, the devil is in the details when it comes to choosing the right piston ring. For one thing, it depends on details such as slot design and fixing groove depth and width. For another, the material plays an important role and affects installation tolerances in its turn. You can find […]

Read more...

Advantages of iglidur® plain bearings in a vehicle interior using the example of backrest adjustment

Jonas Burk | 17. May 2021

The reasons for iglidur® plain bearings in vehicle interiors are manifold. In this blog post, I explain the main advantages based on 5 features. Enjoy reading!

Read more...

Vergrößerte Ansicht eines Metall-Polymer-Lagers im Querschnitt

Plain bearing materials in comparison: metal-polymer plain bearings

Lars Butenschön | 6. May 2021

In this section of our series of articles on the subject of plain bearing materials, we look at the so-called metal-polymer plain bearings. What are metal-polymer plain bearings? How do they differentiate themselves from other types of bearings? What are they particularly good for and when is it better to leave them alone? In this […]

Read more...

How to improve the chain magazine with plain bearings?

Volker Beissel | 24. March 2021

Wherever precision in the µ range is required in the machine tool, plain bearings made of plastic reach their limits. However, in places where this is not the case, they can reduce costs and minimise maintenance. A typical place where our plain bearings show their full strength is in chain magazines of tool changing systems. […]

Read more...