iglidur plain bearings - igus Blog - Page 9 iglidur plain bearings - igus Blog - Page 9

Keyword:

iglidur plain bearings

Three key technical indicators that should always be considered during bearing selection

Lars Butenschön | 19. March 2020

Only one short work step left … and then it happens. The device refuses to work. The knee lever seizes, and the machine performs an emergency stop. The user has just one concern: “How long does the service technician need?” “Why can’t this piece of junk keep it together until I’m done with this urgent […]

Read more...

This is how you protect shafts from wear and corrosion

Lars Butenschön | 12. March 2020

And again the working platform cracks, squeaks and crunches when the hydraulics are actuated. If noise is generated during operation or the device even jams, it is often already too late. Once you (or the appointed service technician) have located and dismantled the bearing, it often flashes and shines at you. Something like that! A […]

Read more...

How do iglidur plain bearings reduce noise in motor vehicles (Buzz, Squeak and Rattle)?

Julio Pauli | 2. October 2019

BSR are all noises that are produced by components and assemblies in the motor vehicle. BSR testing, also called a noise and rattle test, is an acoustic method from the automotive industry and is used to measure the volume of these noises. A realistic situation with corresponding vibrations is simulated and the volume of the noise is then measured. The technical challenge for the vehicle and component engineers is to identify the ‘noisy’ components and replace them with a quieter solution wherever possible.

Read more...