Deep groove ball bearings
Deep groove ball bearings according to DIN 625 standard are the most commonly used ball bearings in industry. Depending on the application, plant operators have different requirements for the installed machine components. For deep groove ball bearings, for example, the possible speeds per minute are usually important. Which ball bearing is suitable for high speeds? And that even made of plastic? xiros is the answer.
Water generators convert the potential energy of water into mechanical or electrical energy. The goal is to make water power usable. This is generally accomplished with dams, turbines in running water, and tidal power plants in seas and oceans. Energy conversion on the oceans and igus’s xiros plastic ball bearings: What do they have to […]
Every normal household in Germany has the problem: plastic bottles pile up and have to be taken to a nearby supermarket. With all the bottles in tow, you head straight to the reverse vending machine, get a receipt, and continue shopping. But close observation reveals a great deal of technology behind the reverse vending machine […]
The most environmentally friendly way to dive is to use flippers. But if you find that too taxing and prefer a certain level of convenience, you can use a pedal-powered submersible. The French adventurer Stephane Rousson, who once crossed the English Channel with a pedal-powered airship, has developed one. “Scubs_x0002_ter“ is the name he gave […]
Ball bearings are our daily bread. As abstruse as this may sound at first, this sentence says how important ball bearings are in our world. Because wherever parts turn, move or rotate, ball bearings, usually also referred to as roller bearings, are used. Without them, the world would literally stand still. Ball bearings are commonplace […]