…be increased chain wear or complete chain failure. It is therefore important that high-quality shaft material and corresponding ball bearings are used. The compensation unit is among the energy chain…
…of the high-quality weld seams. Secondly, our orders from various industries have increased since February 2021. This welcome this positive development.” The self-developed system is particularly suitable for recurring processes…
…bearing alternative: https://www.igus.eu/info/ball-bearings-technology?L=en
The benefits at a glance:
Lubrication-free and low-maintenance Corrosion resistance Metal-free when using glass or polymer balls Temperatures up to +150°C possible High media resistance Lightweight…
…Further information on new products with food certifications can be found under the following links
iglidur A350 filament: https://www.igus.eu/info/3d-printing-high-temperature-food-compliant?L=en iglidur A250 knife edge rollers: https://www.igus.eu/info/material-for-knife-edge-rollers-in-food-industry?L=en iglidur A230 clip bearings: https://www.igus.eu/info/a230-flexible-bearings-for-sheet-metal-in-food-industry?L=en…
…energy chain need autonomous power generation by means of energy harvesting? ← All Topics
To drive itself, the generation power by means of energy harvesting in the new P4HD
…