…lot of moisture/high humidity. iglidur plain bearings are corrosion-free, of course. But is this also true of your shaft? And the housing? This is where the dust mentioned above comes into…
…follow the igus:bike on Instagram or Facebook!
More information about the bike and the project can be found on the igus:bike website.
Or would you like to…
…right material for my application? ← All Topics
In view of the more than 60 different iglidur materials and innumerable plastic or metal plain bearings of other suppliers, it
…
…as a consequence of temporary or long-term temperature effects can also cause jamming. In this case, it is important to pay special attention to the materials used and the tolerances…
…plastics are not nearly as strong as steel and similar materials. Nevertheless, there are iglidur materials that have proven their worth at load bearing points with loads above 150 MPa…