…2203 / 9649-7074 Mobile: +49 – 162 / 6272 697 E-mail: jburk@igus.net
You can find more information about automotive applications here.
Plain bearings | Gears | Rollers | 3D printing | Lead screw technology | Special parts according…
…common: they must function reliably 24 hour a day, seven days a week – ideally for a long period of time. Periodic maintenance is not desirable.
That means that…
…saves time, but also money. Due to the combination of two cables, not only material can be saved in production, but also space and working time during assembly and harnessing,…
…has dedicated itself to making the bicycle run as quietly as possible. With the 3D printing service, the disturbing part was reprinted, but this time from the high-performance plastic iglidur®…
…would fitters buy autoglide 5?
Because it is less work. It is also very simple and not particularly demanding. It leaves more time for more important things on the…