…Extruders are often used in very dusty environments, such as tyre production. Lubrication-free and dust-proof properties have top priority in such operations. Maintenance-free and tribologically optimised polymers from igus fulfil…
…The internal algorithms evaluate exceedances of the threshold resistance in the time context for triggering the potential free contact (OUT1) In addition to the potential free contact, the status is…
…components also plays an important role.
xiros ball bearings made of high-performance polymers are the right choice. They are not only 100% lubrication-free, FDA-compliant and low-maintenance, but they also…
…These mechanical components are largely installed on the bottom of the AGV, where maintenance personnel have difficulty reaching them. The first commandment is therefore “Thou shalt install low-maintenance or maintenance-free…
…with maintenance-free, smooth-running xiros fixed flange ball bearings made of the high-performance polymer xirodur S180. In the past, the rollers were made of colourless anodised aluminium, so the introduction of…