What should I consider for a side-mounted application? - igus Blog What should I consider for a side-mounted application? - igus Blog

What should I consider for a side-mounted application?

Phillip Hagedorn | 7. July 2019

What should I consider for a side-mounted application?

You are here:
e-chain side-mounted gliding

Especially when the installation space is tight, installing a side-mounted e-chain is helpful. It is important to pay attention to whether the e-chain glides on a surface or is designed for unsupported application.

Gliding: If the e-chain is gliding horizontally mounted on the side, special attention must be paid to the following points:

  • Use of locking mounting brackets is recommended.
  • Wear pads should be sufficient.
  • Glide surface can be an igus plastic, stainless steel (material: AISI 304) or a galvanised steel.
  • The “back” of the energy chain should be supported.

Unsupported: If the e-chain is used unsupported side-mounted, the length of the travel depends on the factors such as time, additional load, width of the e-kette, bend radius and parallelism of the application. In addition, the following points must be noted:

  • Feasibility/load in terms of weight (FL90 diagram, please contact us)
  • Use of locking mounting brackets is recommended
  • An e-chain of undercut design is recommended.
  • The first three chain links after the mounting bracket should, for instance, be supported by a plate.

Due to the variety of application possibilities, we strongly recommend that you make use of our consulting services.

You already voted!

Related questions

You are also welcome to comment on the article - we look forward to your opinion!