What is induction brazing and what are its advantages? - igus Blog What is induction brazing and what are its advantages? - igus Blog

What is induction brazing and what are its advantages?

Beke Nieszytka | 25. September 2020

What is induction brazing and what are its advantages?

You are here:

Induction brazing is used for both soft soldering and hard soldering. Here, the required heat is generated by induction in the components. Alternating current flows through the inductor surrounding the solder joint. The changing magnetic field generates a current in the components, which heats them. Due to a suitable design of the inductor, it is possible to heat only the solder joint.
The frequencies used are divided into medium frequency and high frequency. Lower frequencies result in heating of the deeper layers of the parts, whereas high frequencies mainly heat the surface.

Benefits:

  • Short soldering times reduce scaling of the workpieces to a minimum
  • Lower interference with adjacent areas due to local heating
  • Very good automation capacity and high reproducibility
You already voted!

Related questions

No further questions have been recorded yet.
You are also welcome to comment on the article - we look forward to your opinion!