In mounting brackets of energy chains, what does “locking” or “pivoting” mean?

The mounting chain link at the beginning and end of the energy chain can be made as lockingor moving. Pivoting connections are used as standard, but in vertical standing applications locking connections can be used, for instance, to prevent the chain from swinging away. In order to obtain additional stability, the mounting brackets are often additionally bolted and locked to the first chain link.