iglidur materials do not need any additional lubrication – unlike many other plain bearings. The friction between plain bearing and shaft is reduced due to extremely fine particles of solid lubricant that are directly embedded in the material and thus are insensitive to outside influences. Vote Up +0 Vote Down -0You already voted!
For almost every shaft, there are appropriate iglidur materials that are highly wear-resistant, which means they have a long service life – whether the material is aluminium, hardened steel or carbon fibre compound. You can find the best combination in comfort with the help of the iglidur Expert system. The surface of the shaft should not be […]
We have dedicated a special blog article to this topic. Initial lubrication – namely, one-time application of WD-40 when the plain bearings are being installed – improves the wear properties, above all in the so-called running-in phase. However, our plain bearings are by no means dependent on lubrication with WD-40. Vote Up +0 Vote Down […]
No, you do not need that. In monitoring their own production, every entrepreneur can decide for himself how much he wants to digitise and utilise the opportunities offered by the Internet of Things. Not everyone is already connected and not everyone wants to network. Many are concerned about transferring their sensitive company data to external […]
Most often, worn plain bearings are clearly noticeable. Unpleasant squeaks, rattling and clattering of the entire bearing or stiff movement are typical symptoms. If the bearing seizes, there is nothing one can do about it. The plant runs up against the block. It would be nice, of course, if you knew in advance when to […]