What is the maximum tensile force of the e-loop?
The e-loopcombines the advantages of a plastic e-chain with those of a high-tensile Dyneema rope. Ideal for three-dimensional movements. The tensile forces are absorbed by the rope and passed through the mounting brackets into the support structure. As a result, the cables are completely free of strain.
The maximum tensile force is 50 kN