How do I push a pre-load prism carriage into the rail profile? - igus Blog How do I push a pre-load prism carriage into the rail profile? - igus Blog

How do I push a pre-load prism carriage into the rail profile?

Michael Hornung | 30. June 2019

How do I push a pre-load prism carriage into the rail profile?

You are here:

The drylin NV pre-load prism slide consists of an anodised aluminium profile in which a sliding carriage travels in prism geometry. The lightweight linear carriage is made of solid plastic, namely iglidur J polymer. On the bottom on both sides, there are sliding elements with spring pre-tension. The pretension can be felt. The carriage is threaded into the inner geometry and slightly pressed in at the pretension sliding elements.

You already voted!

Related questions

You are also welcome to comment on the article - we look forward to your opinion!

Article keywords:

Prism carriages

Newsletter:

Choose a topic now