Yes. iglidur N54 consists of 54 % renewable raw materials. Vote Up +1 Vote Down -0You already voted!
The adequate bearing clearance is set automatically in the case of iglidur plain bearings – unless agreed otherwise, – for example example, for customised special products that are made – after being press-fitted. This clearance results from the tolerance of the plain bearing (E10, F10 or D11, depending on the material) and the tolerance of the […]
In the case of plain bearings, the shaft moves permanently and is simultaneously in contact with the running surface of the bearing. This means that the nature of the shaft is as important for the service life of the system as that of the plain bearing. Whereas the properties of the plain bearing materials can […]
The maximum long-term temperature for the use of iglidur PRT slewing rings is 180°C with sliding elements made of iglidur H1. Vote Up +0 Vote Down -0You already voted!
Reaming or increasing the hole size of iglidur plain bearings is possible without further ado, and can even have a positive effect on the running-in phase – the frictional properties when the component is in a new condition. Materials with a high fibre content, however, can become rougher or frayed during machining. You can find more […]