An outstanding component of the modular drylin W linear system is the WJ200UMA exchange bearing. With this type of linear bearing, the liner can be changed directly on the rail. No linear housing, no linear carriage, no linear module, no delta robot needs to be removed for this. All four bearings can be replaced in […]
A linear guide made of aluminium, plastic or carbon? But it is not very durable. A linear guide must be made of steel, only then is it any good. And that’s true: In many applications involving the dynamic movement of high loads, linear guides made of steel are the first choice. But times have changed; […]
What do I need a linear guide in a piece of furniture for? Perhaps “furniture fitting” is a better word to describe the task in this context. Furniture is becoming increasingly alterable: it changes seat positions and posture, table heights can be adjusted as required, doors slide ultra-silently, TV monitors are positioned in all directions, […]
In the installation instructions for a lubricated linear guide with ball circulation, the following aspects, among others, need to be considered by me: Installation and maintenance only by specialist personnel – Suitable lifting equipment is to be used – Avoidance of dirt during installation; which leads to questions: How can dirt be removed (benzene or […]
“No room. ” Kitchen appliances, laboratory and analysis systems, 3D printers, furniture, lights and so on should be light and transparent and nevertheless be extremely flexible. And their elements should be easily adjustable, offer a high-quality adjusting feel, cost little money and still take up little installation space – also innovative, by the way, in […]