Will the e-chain function even during cold weather/in combination with snow and ice?
Our energy chains are very robust and even withstand extremely low temperatures below freezing point. Every one of our energy chains is tested in a cold chamber at -40 degrees Celsius in our test laboratory as well as in an outdoor test facility under real conditions. In the event of special requirements, our energy chains are also available in closed systems with a housing. In sluices or sewage treatment plants, for example, our ‘basic flizz’ is recommended.