Plain Bearings - igus Blog - Page 29 Plain Bearings - igus Blog - Page 29

Category:

Plain Bearings

Gleitlager mit Formeln

Calculate surface pressure for plain bearings – this is how it works!

Lars Butenschön | 4. June 2020

One of the most important parameters for determining the correct plain bearing is the surface pressure that occurs in the respective application. Without them, one can actually only roughly estimate (sounds more technical than “guessing”) whether the plain bearing in question is suitable. As a matter of course, literature and the technical documentation of the […]

Read more...

igubal 2.0 – Metal-plastic rod ends are the new star in railway exteriors

Thorsten Mersch | 4. June 2020

In appointments with customers and during discussions at trade shows, our range of bearings with angle compensation is always well received. Lubrication-free and maintenance-free, in addition electrically insulating and vibration dampening. Ideal for solutions in the interior of trains such as seat adjustments. For applications in outdoor areas, the subject of tensile strain and compressive […]

Read more...

Certifications for the food and beverage industry

Jan Michels | 3. June 2020

Since food and beverages are sensitive products, production and processing must also be precisely tailored to them. This applies in particular to direct food contact. For this reason, there are igus materials that have been specifically developed for the requirements of the food and beverage industry. Starting with FDA-compliant, later EU 10/2011-compliant materials were added. […]

Read more...

Gears made of iglidur® high-performance polymers in actuators

Steffen Schack | 2. June 2020

The proportion of electronic and electromechanical components in vehicles has been growing continuously for years. The increased comfort and the growing safety requirements promote this development. The cable harness, which is responsible for supplying all these components, is the second heaviest component in many motor vehicles, right after the engine. Actuators make up a large […]

Read more...

Bonding polymer plain bearings – How it works

Lars Butenschön | 28. May 2020

Plain bearings are usually pressed or clamped into the housing hole. They hold securely in the hole and do not rotate unintentionally. But what if this is not possible due to manufacturing tolerances? Another case: the plain bearing should even rotate. Even if it is not part of the standard repertoire of many plain bearings […]

Read more...