igus:bike world tour – Between Vineyards and Showers – 10 km Through the Heart of the Côte Chalonnaise igus:bike world tour – Between Vineyards and Showers – 10 km Through the Heart of the Côte Chalonnaise

Between Vineyards and Showers – 10 km Through the Heart of the Côte Chalonnaise

Michael Poepke | 14. June 2025

Saturday morning, the igus:bike left the city streets behind and headed for greener – and wetter – pastures. Destination: Burgundy, starting from Givry, a charming little wine village nestled in the heart of the Côte Chalonnaise.

Rolling out through the vines

The day kicked off like a postcard: perfectly aligned rows of grapevines, winding little paths, and that peaceful countryside hush that only early mornings can bring.

10 rainy kilometers on the Greenway

But it didn’t take long for the skies to turn grey. The drizzle set in, and suddenly our ride had a bit more of an adventurous vibe. We covered the 10 km to the South Côte Chalonnaise Tourist Office under a steady, fine rain. The bike? Unfazed. No rust, no squeaks, and still gripping the road like a champ – even when it’s slick. A solid reminder that this bike is built grease-free and weather-resistant.

Arrival at the tourist office

Soaked but smiling, we wrapped up this short stage at the tourist office.
The weather may have cut the ride short, but one thing’s clear: the igus:bike doesn’t shy away from the elements. And neither do we.

Next stop: Annecy – time to take this tour into the heart of the Alps.

You already voted!
You are also welcome to comment on the article - we look forward to your opinion!