All messages - igus Blog - Page 124 All messages - igus Blog - Page 124

Endurance test for the latest P4 generation, P41.80RI roller e-chain on ship unloader crane at EMO B.V.

Jens Göbel | 15. July 2020

The new igus P41.80RI roller chain with integrated iglidur plain bearings has been doing its job on the gigantic ship unloader cranes from EMO B.V. in Rotterdam since the end of 2015. EMO B.V. is one of the largest bulk terminals in Western Europe. With a trolley travel of over 100 m, a travel speed of up to 4 m/sec and an additional load of over 50 kg/m, it is one of the most demanding energy chain applications in the port crane sector.

Read more...

e-spool – the alternative to a cable drum on EOT cranes

Jens Göbel | 15. July 2020

The e-spool is a chain-based drum application without a slip ring. Ideal for applications and lifting devices that have no space for a collection basket (lift band). The cables routed in the chain are not exposed to tensile stress, which has a positive effect on the service life of the cables.

Read more...

Linearachsen mit Spindelantriebe oder Zahnriemenantrieb

Which linear axis drive is the right one for me?

Thomas Urbach | 15. July 2020

Linear axes and linear modules can be driven differently. Which system is the right one for me – lead screw drive or toothed belt drive?

Read more...

Lead screw technology in the DIY beer lift

Zoe Moser | 13. July 2020

A decisive point for the smooth application of the beer lift is the use of the correct high-helix thread system. The length of the lead screw is approx. 1 metre. In order to be able to guarantee the service life as long as possible, there are two important points to consider.

Read more...

CF-Blog_Fertigungsstraße

Why flexible cables are not a wear-resistant part

Stefan Wehrmann | 13. July 2020

Production processes can be clearly and easily perfected by using cables that are optimised for the application. Otherwise, supposedly cost-effective wear-resistant parts quickly turn out to be hidden cost traps.

Read more...