All messages - igus Blog - Page 110 All messages - igus Blog - Page 110

The time for heating begins: polymer ball bearings from igus® defy extreme heat

Patrick Czaja | 27. October 2020

Plastics and hot temperatures in ovens do not have to oppose each other, as shown in the following application example of the Koppe company. Because lubrication-free polymer ball bearings from igus are successfully used in their pellet stoves for private households. The functionality of the stoves is ingenious, as the pellets burn without electricity via a mechanical drive unit. The polymer ball bearings ensure long running times and smooth operation in the drive unit.

Read more...

Which igubal® housing material is most suitable for my application?

Peter Hughes | 26. October 2020

As with all igus® products, the igubal® spherical bearings come in a wide range of materials. Each material is designed to suit specific requirements, whether you require a rod end for high-temperature environments or a flange bearing for food contact. Here we will provide you with an overview of the materials available, and their uses. […]

Read more...

ATEX certification for machines in explosion risk areas with 3D printing of ESD special parts

igu-blog-adm | 26. October 2020

Even a small spark in a potentially explosive atmosphere, can have devastating consequences for personnel and the entire plant. However, friction – especially friction of moving plastic components against each other – causes sparks. In order to permanently protect these components from irreversible damage, a controlled discharge is necessary. This means that materials with defined […]

Read more...

How to connect the igus Robot Control to your PC

Adriana Glazer | 23. October 2020

When purchasing various robot kinematics, igus Robot Control is optionally available as a switch cabinet version or top hat rail version and offers the user an easy entry into automation. The various robot kinematics can be connected quickly and easily via an Ethernet interface between the control system and the PC. In this article you […]

Read more...

Can I lubricate plastic plain bearings with WD-40? – iglidur plain bearing podcast – episode 01

Lars Butenschön | 21. October 2020

Quite often squeaking plain bearings are treated with WD-40. But what works for creaking living room doors or rattling bicycle chains can’t hurt plain bearings, right? I will get to the bottom of this question in today’s podcast episode. Further information on the topic: The detailed background to our laboratory tests with WD-40 and plastic […]

Read more...