What is the upper run of an energy chain? - igus Blog What is the upper run of an energy chain? - igus Blog

What is the upper run of an energy chain?

Marco Thull | 5. July 2019

What is the upper run of an energy chain?

You are here:

The upper run is the upper part of an energy chain. In a horizontal linear motion, the length of the upper run changes continuously. For this reason, the maximum unsupported upper run length must be taken into account in a horizontal application. This depends on the chain series, the additional load and the max. speed/acceleration. To determine these lengths, manufacturers of energy chains have load diagrams for each chain series.

A so-called load diagram for an energy chain
You already voted!

Related questions

You are also welcome to comment on the article - we look forward to your opinion!

Article keywords:

Long travel Short Travel

Newsletter:

Choose a topic now