June, 2020 - igus Blog - Page 6 June, 2020 - igus Blog - Page 6

Polymer bearings in spring-mounted seat posts

Alexander Muzicenko | 5. June 2020

The seat post is an important component of a bicycle, especially when it comes to comfort. Not all roads are level and every impact is passed on to the rider. The saddle alone cannot absorb all impacts. The loads without suspension can have serious consequences for the back, for example. Essentially it is about more […]

Read more...

Precise polymer bearing points in medical technology

Ulf Hottung | 5. June 2020

“Can’t be done!” say many design engineers and are therefore not generally wrong, but also not always right, especially in medical technology. Correct is: polymer bearings, or bearing points in polymer in general, are subject to various factors that influence the preferred bearing clearance. Impact on precision Correct is: polymer bearings, or bearing points in […]

Read more...

Gleitlager mit Formeln

Calculate surface pressure for plain bearings – this is how it works!

Lars Butenschön | 4. June 2020

One of the most important parameters for determining the correct plain bearing is the surface pressure that occurs in the respective application. Without them, one can actually only roughly estimate (sounds more technical than “guessing”) whether the plain bearing in question is suitable. As a matter of course, literature and the technical documentation of the […]

Read more...

igubal 2.0 – Metal-plastic rod ends are the new star in railway exteriors

Thorsten Mersch | 4. June 2020

In appointments with customers and during discussions at trade shows, our range of bearings with angle compensation is always well received. Lubrication-free and maintenance-free, in addition electrically insulating and vibration dampening. Ideal for solutions in the interior of trains such as seat adjustments. For applications in outdoor areas, the subject of tensile strain and compressive […]

Read more...

Cables for crane applications

Theo Diehl | 3. June 2020

A wide variety of cables are used in modern crane systems. The load due to constant movement is the same for all trolley and crane supply cables.

Read more...