For pivoting and rotary movements of up to 270°, it is important that cables and hoses are laid in the energy chain’s neutral phase. Why is this so important? Pivoting and rotary movements usually involve winding up the e-chain or guiding it into an S shape. For normal installation positions (horizontal, standing, or suspended), the […]
The cable guide problem can be solved with an energy chain on indoor cranes with two trolleys as well. But two trolleys must not always be the reason for a reverse energy chain application.
A tooth breaks on a gear, and that’s all it takes to stop the machine. Unfortunately, the documentation has been lost, and the manufacturer does not supply spare parts any more and may even have gone out of business. What now? The gear must be replaced, and there are no clues besides the broken component. […]
The great demand means that machine tools are often mass-produced. It is especially important that each machine – whether it is a milling, turning, grinding or drilling machine – is identical with respect to quality and precision.
In large machines, the X-axis is always a particularly great challenge. All supply lines the machine requires run through this e-chain, which can be very long. That is why reliability is especially important here. Because each machine tool is unique, we always try to find the best solution for the application in question. The […]