In most cases, an installation of insulation displacement termination works smoothly and without special cables. In exceptional cases there may be small hurdles, which we will discuss in more detail today. The interaction of insulation displacement terminations and cables is important. What is an insulation displacement termination and how does it work? The technology of […]
The cable guide problem can be solved with an energy chain on indoor cranes with two trolleys as well. But two trolleys must not always be the reason for a reverse energy chain application.
For pivoting and rotary movements of up to 270°, it is important that cables and hoses are laid in the energy chain’s neutral phase. Why is this so important? Pivoting and rotary movements usually involve winding up the e-chain or guiding it into an S shape. For normal installation positions (horizontal, standing, or suspended), the […]
The decisive factors in today’s plastic processing industry are efficiency and productivity. That is why automation processes such as machine feeding, component handling and pick-and-place processes are essential components of modern, economic production. Automation made easy with igus Low Cost Automation.
For historical reasons, energy chains have so far always been manufactured from steel or plastic. Steel has the advantage of allowing longer unsupported lengths. A plastic energy chain has various advantages, including lower cost and faster installation. There is now a new product: the hybrid steel-plastic chain. The energy chain is built with steel inner […]