The autoglide 5 lasts longer than you think …
Christian Strauch | 16. May 2022
One might think that I would have said everything you could say about the autoglide 5 by now, but I haven’t come close.
The autoglide 5 still has some advantages over the basic chain, including the following:
The autoglide 5’s special crossbars increase the load-bearing surfaces or sliding surfaces. Larger sliding surfaces also mean lower surface pressure for the same weight, which in turn means a longer service life given the same parameters.

We have tested it for you in our 3,800m² laboratory, of course.

Depending on the speed and cable filling (that is, the additional weight per metre), the service life increased by at least 20%. In some cases, the increase was as high as 60%.
Conclusion: Lose the busbar system and get the autoglide 5!
You are also welcome to comment on the article - we look forward to your opinion!