Xiros - igus Blog - Page 5 Xiros - igus Blog - Page 5

Keyword:

Xiros

The time for heating begins: polymer ball bearings from igus® defy extreme heat

Patrick Czaja | 27. October 2020

Plastics and hot temperatures in ovens do not have to oppose each other, as shown in the following application example of the Koppe company. Because lubrication-free polymer ball bearings from igus are successfully used in their pellet stoves for private households. The functionality of the stoves is ingenious, as the pellets burn without electricity via a mechanical drive unit. The polymer ball bearings ensure long running times and smooth operation in the drive unit.

Read more...

4 interesting facts about ball bearings that will surprise you

Patrick Czaja | 9. September 2020

What does a famous painter, children’s toys and a bicycle road race have in common? For some, this is surprising, but they are in some way associated with ball bearings. When you think about ball bearings, many people know that they are mainly used in industry, such as in factories and motor vehicles. Rolling bearings […]

Read more...

xiros guide rollers for labelling technology: quiet, safe & effortless guidance

Patrick Czaja | 20. August 2020

The xiros guide rollers have been in the igus range for a while. They modestly, discreetly and quietly improve various applications in the background. Our rollers are constantly being further developed and improved to ensure that their flexibility is suitable for numerous applications and industries. Our black anodised guide roller for visible parts expands the […]

Read more...

Why lubrication-free is a better option for your ball bearing

Patrick Czaja | 15. June 2020

Grease or lubricating oil is essential for installing metal ball bearings. With xiros polymer ball bearings you can enjoy 100% lubrication-free ball bearings made of plastic. No grease No oil No residues on hands or machines! In most applications where ball bearings are used, mainly low loads and low speeds are required. Plastic ball bearings can be used in multi-functional applications, for example, in cases where they come into contact with liquid media, water or chemicals.

Read more...

Save lubricant, prevent contamination & increase the service life of ball bearings

Patrick Czaja | 5. June 2020

Contaminated lubricant is one of the main causes of bearing damage and often a major factor in the premature end in the service life of bearings. Around 70% of bearing failures are caused by lubricant problems, such as contamination in the lubricant (25%), incorrect lubricant (20%) or too little lubricant (14%).

Read more...