Xiros - igus Blog - Page 3 Xiros - igus Blog - Page 3

Keyword:

Xiros

Why your ticket machine ball bearings should be from igus®

Patrick Czaja | 7. January 2021

Ball bearings in ticket machines where requirements for installed components are stringent. igus polymer ball bearings are expanding their advantage over metal ball bearings in this segment. They are not only maintenance-free and lubrication-free – they also ensure that the application environment is free of contamination. Searching for contamination of tickets and banknotes: not here

Read more...

Ball bearings in material handling: why igus® ball bearings are the ones to beat

Patrick Czaja | 5. January 2021

There are two decisive arguments for efficient material handling: freedom from lubrication and freedom from maintenance. Ball bearing reliability and load capacity in material handling are also necessary to ensure smooth running.

Read more...

igus® impresses with ball bearings in hose pumps

Patrick Czaja | 17. December 2020

The general requirements for the bearing components used in medical and food technology are extremely high and are subject to high quality standards. For example, in medical diagnostics such as dialysis, it is important to have components that are 100% free of lubricating greases or oils in order to keep the application sterile and clean.

Read more...

Ball bearings in the textile industry – why plastic beats metal

Patrick Czaja | 10. December 2020

Textile machines and their components are increasingly exposed to heavy loads. This increases the demands on the machines. Vibrations, different operating conditions, constantly changing loads and especially dirt and dust adhesion are challenges faced by plant operators in the textile industry.

Read more...

Ball bearings in anemometers – plastic makes measuring wind easy

Patrick Czaja | 8. December 2020

An anemometer is an instrument for measuring the speed of a flow field and is used primarily to determine wind speed. The cup anemometer is the most widely used type. It has a vertical axis with three or four cups to catch the wind. What requirements apply to ball bearings in anemometers?

Read more...