robolink®
The AS5304A linear encoder chip of the manufacturer Austriamicrosystems is located on the sensor boards. The magnetic rings have 31 pole pairs (pivot) and 29 pole pairs (rotation), so that 4960 (pivot) and 4640 (rotation) signals respectively are issued per rotation. This corresponds to an angular accuracy of approx 0.07°. In addition, our magnetic rings […]
Available now, produced by laser-sintering process With the new product configurator, you can now request for a customized system quickly and easily. Configure individually from the robot joint kit and inquire or order directly online. robolink configurator Vote Up +0 Vote Down -0You already voted!
robolink news and line extentions, more joints, connecting pipes and much more. Vote Up +0 Vote Down -0You already voted!
Robolink has been awarded by the “iF Forum Design GmbH” in the category “industrial design”. The iF awards are given particularly to innovative and visually appealing products. As one of the oldest competitions, the iF award is an internationally recognized design award. Award-winning igus® designs Vote Up +0 Vote Down -0You already voted!
angular sensor Due to the integrated angular sensors, an arm can also be used directly as “teach-in” arm. Read-out angle information can be saved and called up or even directly transformed into movements (see film). Currently the sensor technology is advanced for series production. Development partner EvoLogics GmbH is a specialist for bionic inventions (the […]