Polymer ball bearings - igus Blog - Page 6 Polymer ball bearings - igus Blog - Page 6

Keyword:

Polymer ball bearings

Why is thermal management becoming more and more significant for the automobile industry?

Sebastian Bloechl | 2. April 2020

Cosy heating in the winter and an air-conditioned living room in the summer – in addition to such everyday concerns, thermal management plays a decisive role in the automotive industry. In that industry, for instance, it is the engine that meets various scenarios. At first, it needs a temperature rise that is as quick as […]

Read more...

What materials are used to make ball bearing balls?

Patrick Czaja | 26. March 2020

The material for rolling bearing ball bearing balls varies widely and is always primarily focused on the ring materials. This ensures that the interplay of cage, inner ring, and outer ring in the system is harmonised. This is especially important when the application involves heating or cooling the bearings. It is important that ball bearing […]

Read more...

Which sealing variants are available for ball bearings?

Marco Thull | 20. December 2019

Many metallic rolling bearings are available as a sealed version The sealing is usually absolutely necessary for metallic ball bearings as otherwise dirt can get into the ball running surfaces, mix with the lubricant and thus block the rolling of the bearing. Metallic bearings must be protected Metallic ball bearings are also available in an […]

Read more...

What is DIN 625?

Marco Thull | 19. December 2019

The DIN 625 specifies the dimensions for single row radial deep groove ball bearings. It is the best known standard in the rolling bearing sector. Radial ball bearings (see picture) are among the most commonly used ball bearings and are designed to support predominantly radial forces. In addition to DIN 625, there is a separate […]

Read more...

When do I use a particular ball bearing? – Metal, plastic, ceramic

Patrick Czaja | 18. November 2019

Choosing the right material for ball bearings is not always easy. A short summary, when I use a particular ball bearing. Limits of metallic ball bearings Metallic ball bearings are mainly used in most classic mechanical engineering applications. They rank number 1 in terms of global sales volumes and are suitable for a large number […]

Read more...