Plastic ball bearings - igus Blog - Page 3 Plastic ball bearings - igus Blog - Page 3

Keyword:

Plastic ball bearings

Which ball bearing seals are available and why doesn’t igus need additional markings

Patrick Czaja | 13. November 2020

Many metallic rolling bearings are available as a sealed version Ball bearing seals are usually mandatory for the metallic version, otherwise dirt will get into the running surfaces of the ball. They can combine with the lubricant and block the bearing run. Ball bearings made of polymer or ceramic are mostly only available as an open type. Why? Find out here.

Read more...

How do I find out the DIN installation size of the metal ball bearing? And how do I find the igus® counterpart?

Patrick Czaja | 11. November 2020

For metallic ball bearings, determining the installation size is usually simple. Usually the type designation is printed either on the inner or outer ring. It becomes more difficult, however, if the imprint remains unrecognisable despite cleaning. Therefore the ball bearing must be measured manually at this point. _x000D_   I now know my ball bearing […]

Read more...

The time for heating begins: polymer ball bearings from igus® defy extreme heat

Patrick Czaja | 27. October 2020

Plastics and hot temperatures in ovens do not have to oppose each other, as shown in the following application example of the Koppe company. Because lubrication-free polymer ball bearings from igus are successfully used in their pellet stoves for private households. The functionality of the stoves is ingenious, as the pellets burn without electricity via a mechanical drive unit. The polymer ball bearings ensure long running times and smooth operation in the drive unit.

Read more...

4 interesting facts about ball bearings that will surprise you

Patrick Czaja | 9. September 2020

What does a famous painter, children’s toys and a bicycle road race have in common? For some, this is surprising, but they are in some way associated with ball bearings. When you think about ball bearings, many people know that they are mainly used in industry, such as in factories and motor vehicles. Rolling bearings […]

Read more...

xiros guide rollers for labelling technology: quiet, safe & effortless guidance

Patrick Czaja | 20. August 2020

The xiros guide rollers have been in the igus range for a while. They modestly, discreetly and quietly improve various applications in the background. Our rollers are constantly being further developed and improved to ensure that their flexibility is suitable for numerous applications and industries. Our black anodised guide roller for visible parts expands the […]

Read more...