Plain bearing applications
The demand for electric water pumps is huge. In addition to the cooling of motors and drives, air conditioning is also one of its tasks. The advantages of electric coolant pumps compared to conventional mechanical water pumps are their independence from the combustion engine. In this way, the electric pumps can be switched on and […]
Maximum vehicle efficiency requires harmonised thermal management. Optimum operating temperature ensures efficiency and thus the lowest consumption and associated emissions. Coolant plays an important role – it cools, provides corrosion protection and prevents frost. Coolant pumps, regulators and valves distribute coolant throughout the vehicle, sending it where it is needed. Find out more here. In […]
Cosy heating in the winter and an air-conditioned living room in the summer – in addition to such everyday concerns, thermal management plays a decisive role in the automotive industry. In that industry, for instance, it is the engine that meets various scenarios. At first, it needs a temperature rise that is as quick as […]