Metal ball bearing – igus Blog

Keyword:

Metal ball bearing

How do I mount ball bearings?

Patrick Czaja | 29. October 2021

If the metal ball bearing is a fixed or floating bearing, the outer and/or inner ring are firmly connected to the shaft or housing. The easiest way to mount this type of bearing is to press it into place. However, certain tolerances are necessary in the dimensions for the shaft and housing. In general, it […]

Read more...

Polymer ball bearings in plasma technology

Patrick Czaja | 12. May 2021

Within the industry, plasma technology has established itself as a technical standard for optimising material surfaces. Atmospheric pressure plasmas are created, for example, by electrical discharges in the air or by other gases. They enable remarkable material surface treatment due to a large amount of reactive and short-lived chemical species. The species clean, disinfect and […]

Read more...

Why metal ball bearings reach their limits in latex processing

Patrick Czaja | 7. April 2021

Whether at the largest manufacturer of rubber gloves in Malaysia or at a specialist in the packaging process of condoms in Thailand: machines in latex processing depend on durable and fail-safe components to avoid downtime. Metal ball bearings are used in a wide range of applications. However, the deployment could turn out to be a […]

Read more...

Ball bearings in sun shades: successful sun protection

Patrick Czaja | 19. March 2021

Spring is approaching, the weather is getting better and the hours of sunshine are increasing again. Especially in summer, when heat is an added factor, sun shades play an important role. The reliable shading of a room not only ensures a pleasant working atmosphere, for example when working on a home computer, but also an […]

Read more...

When should I change my ball bearing?

Patrick Czaja | 11. February 2021

The defect of a ball bearing can have various causes; whether cage wear, ball breakage or damage to the running surfaces. Find out in this blog post why igus can be an alternative to metal after a defect.

Read more...