Maintenance-free - igus Blog Maintenance-free - igus Blog

Keyword:

Maintenance-free

Save grease effectively with lubrication-free spherical insert bearings!

Tom Schrage | 3. August 2022

Our world is constantly on the move and the machines that meet our needs are running around the clock. And regardless of whether it is guide rollers, construction machines or robots, where things are in motion, there is friction between the materials, which in some cases are exposed to high loads as a result. Every […]

Read more...

Ball bearings in small sewage plants

Patrick Czaja | 9. June 2021

In many cities and towns, it is completely normal for houses and flats to be connected to the public sewage system. Wastewater is sent to a central sewage plant, where it is cleaned. But this solution is not universal. Very small settlements and outlying houses are usually dependent on their own solutions. They have no […]

Read more...

Why your ticket machine ball bearings should be from igus®

Patrick Czaja | 7. January 2021

Ball bearings in ticket machines where requirements for installed components are stringent. igus polymer ball bearings are expanding their advantage over metal ball bearings in this segment. They are not only maintenance-free and lubrication-free – they also ensure that the application environment is free of contamination. Searching for contamination of tickets and banknotes: not here

Read more...

The time for heating begins: polymer ball bearings from igus® defy extreme heat

Patrick Czaja | 27. October 2020

Plastics and hot temperatures in ovens do not have to oppose each other, as shown in the following application example of the Koppe company. Because lubrication-free polymer ball bearings from igus are successfully used in their pellet stoves for private households. The functionality of the stoves is ingenious, as the pellets burn without electricity via a mechanical drive unit. The polymer ball bearings ensure long running times and smooth operation in the drive unit.

Read more...

Lead screw technology in the DIY beer lift

Zoe Moser | 13. July 2020

A decisive point for the smooth application of the beer lift is the use of the correct high-helix thread system. The length of the lead screw is approx. 1 metre. In order to be able to guarantee the service life as long as possible, there are two important points to consider.

Read more...