e-spool power
The e-spool is a chain-based drum application without a slip ring. Ideal for applications and lifting devices that have no space for a collection basket (lift band). The cables routed in the chain are not exposed to tensile stress, which has a positive effect on the service life of the cables.
The e-spool is a chain-based drum application without sliding contacts. Ideal for applications and load-carrying equipment constructions that have no room for a collection basket (lift strap). The cables guided in the chain are not exposed to tensile strain, which has a positive effect on the service life of the cables.