development - igus Blog - Page 11 development - igus Blog - Page 11

Keyword:

development

Feedthrough of draw wires

Martin Raak | 27. February 2012

For the series connection of joints, the 4 draw wires of the second (or upper) joint should be conducted through the first (or lower) joint. This feedthrough must be done in such a way that a movement of the lower joint does not alter the wire lengths of the feedthrough, which means Bowden cables are […]

Read more...

Tensile strength test report of robolink® wires

Martin Raak | 26. January 2012

robolink® wires were tested for tensile strength on the ZWICK tractor (nominal tensile strength > 3600 N).The nipple connection was fixed with different adhesives (see installation instructions for the wires). The experiments were carried out at room temperature and at 80°C.          Wire with brass nipples  Section of the mounted nipple Test […]

Read more...

Angular sensor

Martin Raak | 1. June 2010

angular sensor Due to the integrated angular sensors, an arm can also be used directly as “teach-in” arm. Read-out angle information can be saved and called up or even directly transformed into movements (see film). Currently the sensor technology is advanced for series production. Development partner EvoLogics GmbH is a specialist for bionic inventions (the […]

Read more...

Development status

Martin Raak | 23. March 2010

Increase in the transmitted torque (rotation) from 5 (generation 1) to 7 Nm (generation 2) in continuous operation. (Damage in the one-off fracture test at > 24 Nm) GFRP and CFRP rods now available in profiled version. Maximum length of 1 m. See price list. Weight CFK: 170 g/m, GFK: 200 g/m, Aluminum 270 g/m […]

Read more...

Current status of the product development

Martin Raak | 14. December 2009

The revised, new version of the articulated robot joint is now available as a prototype. The following product improvements have been achieved: lower cable friction due to less narrow cable guide for the rotational motion (newly laid Bowden cables with optimized friction couple => see figures) New design of the transition from articulated joint to […]

Read more...