Corrosion-free
Warm summer evenings, starry skies and marvelling at a choreography with colourful water fountains and walls supported by music – a great feeling. However, there is quite a bit of technology behind this breathtaking light and water show. If there is a technical error or even a defect in the components, the choreography can quickly […]
The adjustable seat post is another variation of the seat post and is also called Dropper Post or Vario. This type is mainly used in mountain biking and has the advantage of height adjustment, which can be operated by remote levers. For downhill riding, the support can be lowered and raised for uphill or normal […]
The seat post is an important component of a bicycle, especially when it comes to comfort. Not all roads are level and every impact is passed on to the rider. The saddle alone cannot absorb all impacts. The loads without suspension can have serious consequences for the back, for example. Essentially it is about more […]
In the bicycle industry, innovative solutions are not only focused on design, but also on the choice of materials. For example, for the frame there are many solutions made of aluminium or glass fibre reinforced material. Component manufacturers are also working flat out on the use of alternative materials. Be it saddle post, suspension, pedals […]
The bicycle is still very popular as a means of transportation. But whether the bike in question is a lifestyle product or a racing machine, the quality challenges for each component are great. Many technical components have profound effects on quality. There are shock absorbers and gear and brake components, of course, but bicycle pedals […]