Control device
In order to control the hoist on the indoor crane, a manual control unit, also known as a control device, is required. It can be moved along the crane girder independently of the hoist. This is to prevent people from standing below or in direct proximity to the lifted load when operating the indoor crane. With the guidefast control system there is also a suitable energy chain solution for such applications. The guidefast control system is installed directly on the crane girder and ensures a safe guidance of the control cable.