cable drum
The e-spool is a chain-based drum application without a slip ring. Ideal for applications and lifting devices that have no space for a collection basket (lift band). The cables routed in the chain are not exposed to tensile stress, which has a positive effect on the service life of the cables.
The lift band was specially developed for vertical applications on indoor / EOT cranes. A spiral energy chain that can be stored in a collecting basket. The cables are routed through the spiral energy chain without being exposed to any tensile stress. The retainer belts attached to the system ensure that the energy chain is safely stored in the special basket. The system is light, requires very little space on the lifting device and it is almost maintenance-free.
The e-spool is a chain-based drum application without sliding contacts. Ideal for applications and load-carrying equipment constructions that have no room for a collection basket (lift strap). The cables guided in the chain are not exposed to tensile strain, which has a positive effect on the service life of the cables.
A stage setting like this in a theatre or opera house is an impressive view every time you see it. There are a lot of lights and hidden technology, which require a certain degree of cable management to achieve. As it is with most stages, the available space which can be used to guide and […]