…will go with “MPa” (Megapascal, 1000 Pascal). 1 MPa are equal to 1 Newton (N) per mm² surface. For the aforementioned man with the hydraulic cylinders and his 30 MPa…
…outdoor area of 2,000m² for long travels and a climate chamber with -40°C, which we are particularly proud of. Here we simulate environments in which they are to be used,…
…mention the fact that manufacturers gain a real competitive advantage through machines that are easier to clean.
Thank you, Mr. Sund!
You’re welcome.
…
…determined. This is possible when systems are equipped with sensors that report wear and workload on the components. Ideally, an IoT online connection compares specified runtime data and real usage…
…machine downtime. The basis for this are status values, which are determined by the i.Sense CF.D sensors from the physical specifications of the data transmission. The real-time evaluation in the…