…wire is applied to the solder joint, where this fuses and melts at the joint. After removing the soldering iron, the solder joint hardens.
Benefits:
Development of a persistent…
…For higher temperatures, people refer to the process as high-temperature soldering or even welding. While with soldering, only the solder is melted to connect parts; with welding, the metals that…
Furnace brazing is a soldering method in which the parts to be joined are heated in an oven with the brazing solder inside, and which is
…
…with different contact inserts. These in turn combine with various connection techniques of crimp, cage clamp, winding connection via solder, axial, quick and IDC connection up to the axial spring…
…components. Alternating current flows through the inductor surrounding the solder joint. The changing magnetic field generates a current in the components, which heats them. Due to a suitable design of…