…Cable attenuation means reduction of the energy of a signal transmitted over a distance and has an effect on the transmission speed in the case of bus cables, for example….
…soldering or high-temperature soldering over 900°C.
Benefits:
Precise dosing of the supplied energy possible Adjacent areas around the solder joint are insignificantly affected Vote Up +2 Vote Down -0You…
…Why “plastics”? igus manufactures components for moving applications from high performance plastic. And these can be integrated in a smart production monitoring system with the appropriate sensors.
Smart…
…influence they exert. ThePUR & iguPUR mixtures have good resistance to many different types of oil. For more aggressive media such as bio-oils, ammonia and so on, TPE material is…
…tools there are many adjustments for height and width. There you will often find entire lead screw modules or toothed belt axes based on drylin W aluminium profile rails. The…