The iglidur Expert tells me that W300 and J are the most long-lasting materials. Which one should I take? - igus Blog The iglidur Expert tells me that W300 and J are the most long-lasting materials. Which one should I take? - igus Blog

The iglidur Expert tells me that W300 and J are the most long-lasting materials. Which one should I take?

Lars Butenschön | 2. July 2019

The iglidur Expert tells me that W300 and J are the most long-lasting materials. Which one should I take?

You are here:

Both iglidur J and iglidur W300 belong to the most wear-resistant all-round bearings in the iglidur product range. If the service life is comparable and sufficient in both cases, the boundary parameters of the application should be decisive for the choice of material: iglidur J is predestined for wet areas due to its low moisture absorption and good resistance to media, whereas iglidur W300 is better able to cope with different temperatures.

You already voted!

Related questions

You are also welcome to comment on the article - we look forward to your opinion!