Upper run - igus Blog Upper run - igus Blog

Tag: Upper run

Why do I have to lower the suspension point in a long travel?

Phillip Hagedorn | 3. July 2019

A lowered connecting point is absolutely necessary for every gliding application: To prevent chain breakage through critical sag. To reduce wear (if the moving end is not lowered, there is more abrasion) Example: If we move the e-chain from right to left till the gap between the upper run and the lower run is 1mm, […]

Read more...

Why is an angled moving end bracket beneficial?

Phillip Hagedorn | 3. July 2019

With a mounting angle between 3-5°, the e-chain is slightly forced downward by the push/pull force. This prevents the rising up of the e-chain. The angle of incidence of the upper run to the lower run is approximately 3-5°. This angle is also ideal for reducing wear. If the upper run is installed in parallel […]

Read more...