Test - igus Blog Test - igus Blog

Tag: Test

How are iglidur plain bearings tested?

Lars Butenschön | 9. July 2019

In addition to the tests carried out in the framework of the material quality inspection, iglidur plain bearings are subjected to special wear tests by igus. Every iglidur material is tested for its wear properties in hundreds of stress scenarios, whereby different plain bearings with diverse dimensions are tested. The data are recorded systematically and are the […]

Read more...

How are harnessed igus cables tested?

Beke Nieszytka | 8. July 2019

After harnessing, all cables pass through our test field. Depending on the specification, various tests can be carried out here. igus works on 10 test fieldswith 3,000 different test adapters. The following tests among others are performed: Digital logic tests High-voltage tests Network tests Attenuation tests Upon request: Customised tests After each test, the associated […]

Read more...

Can igus energy chains be used in the refrigeration sector?

Marco Thull | 3. July 2019

Yes, all igus energy chain materials can be used for continuous use down to -40°C. Vote Up +1 Vote Down -0You already voted!

Read more...

Will the e-chain function even during cold weather/in combination with snow and ice?

Marco Thull | 1. July 2019

Our energy chains are very robust and even withstand extremely low temperatures below freezing point. Every one of our energy chains is tested in a cold chamber at -40 degrees Celsius in our test laboratory as well as in an outdoor test facility under real conditions. In the event of special requirements, our energy chains […]

Read more...